4431-T-B1_B_915

Changes compared to the previous version:

V2.0 - 13/01/2011

Component values in the schematic were modified (according to AN427 Rev0.1):
	
	- Value of the LR inductor was changed from 10nH to 11nH
	- Value of the CR1 capacitor was changed from 3.9pF to 3.3pF
	- Value of the CR2 capacitor was changed from 8.2pF to 6.8pF

General Manufacturing pack update:
	
	- manuf. notes were updated
	- component attributes were updated
	- BOM was updated